RFID (Radio Frequency Identification) is a contactless auto-ID technology. It uses RF (LF, HF, UHF or microwave) signals to implement a contactless communication between RFID reader and tags so as to automatically identify the targets and obtain data.
A complete RFID system is made up of tags (transponders), RFID reader, and host system. The tags (transponders) play the role of information carriers of RFID systems. Each tag has a unique electronic series code embedded in it. [+MORE]
The RFID reader is used to read the information in tags, and then send it to host systems if the identity of a tag is approved. Typically a RFID reader is composed of RF antenna, transceiver, MCU and peripherals. The peripherals include communication interfaces (RS232 or USB), human-machine interface (keypad, LCD display, LED lights and buzzer/speaker), and actuating mechanism (motor or solenoid valves). Some of them are optional ones depending on specific applications. The host system is responsible for processing the received information.
According to the tags, RFID systems can be divided into passive RFID, active RFID, and semi-active RFID types. The major difference among these types lies in the power supply of their tags. RFID systems can also be grouped by their operation frequencies including LF (Low-Frequency at 125 KHz and 134.2 KHz), HF (High-Frequency at 13.56 MHz), UHF (Ultra-High-Frequency from 860 MHz to 960 MHz), and MW (Microwave at 2.4 GHz and 5.8 GHz). Different frequencies results in different working principles, suited applications, effective transmission range, and transmission speed of RFID systems.
Currently RFID technology has been used in a diversity of applications such as animal ID, transportation payment, access and security, asset management and retail sails, product tracking, promotion tracking, inventory systems, and libraries. And a very interesting application of this technology called payment by cell phones has been widely spread around the world in recent years.[-LESS]
Hover over the blocks to view more recommended solutions
| |
 |
RI-STU-MRD1-30
TEXAS INSTRUMENTS
The Series 2000 Micro Reader provides all RF and control functions to communicate with 134.2 kHz HDX/FSK transponders and a host application, on a 30-pin Dual in-line pcb profile. Its equipped with a serial communication interface that works in combination with a low-Q antenna, eliminating the need to tune the system to resonance. It converts the received RF signals to the transponder's id number, validites and handles the conversion to the RS232 serial interface protocol. |
|
| |
 |
EURIDK4917
AVONWOOD
The Eureka UHF active RFID Kit is supplied with an RF reader, wake-up units, cables, tags, software and manuals. The active tag reader is a self-contained unit with 868MHz PCB dipole antenna that decodes/detects iD tags, communicates via TCP/IP over LAN connection, capabble of detecting tags upto 100m in free air. |
|
| |
 |
EURUHFK4915
AVONWOOD
The Eureka UHF passive RFID Kit provides an ideal introduction to the technology, supplied with a reader unit, cables, tags, software and manuals. It's a 4-port reader - a multi-protocol starter kit, capable of long range programming and reading UHF tags. |
|
| |
 |
RWD-MIFARE-OEM
RF SOLUTIONS
RWD-MIFARE is a complete RFID reader and tag acceptance solutionfor 13.56 MHz Mifare (1k and 4k byte versions) and Mifare Ultralight cards. The reader will support any RFID tags using this protocol including CARD-MIFXK transponder cards. Also a wide variety of tag types are available which support this protocol. The RFID receiver only needs an antenna connected and 5v DC supply to be a fully featured ISO14443A Mifare read/write system.
|
|
| |
 |
EB539
MATRIX
The Kit includes everything needed for rapidly development of RFID based systems linked to microcontroller hardware. A copy of Flowcode (macros included for rapid RFID development), an E-blocks PICmicro microcontroller USB multiprogrammer, LCD board, LED board, switch board, RFID board, power supply, 2 Mirfare type RFID cards and a spare 16F877A device are included.
|
|
| |
| MICROCHIP |
Transmitter |
MF RM700 Antennas and matching adapter description |
|
|
Click Here |
| MICROCHIP |
Transmitter |
Interface Control Document for the 13.56 MHz Anti-Collision |
AN759 |
MCRF4XX |
Click Here |
| MICROCHIP |
Transmitter |
Low-Frequency Magnetic Transmitter Design |
|
|
Click Here |
| MICROCHIP |
Transmitter |
Antenna Circuit Design for RFID Applications |
|
|
Click Here |
| MICROCHIP |
Transmitter |
RFID Coil Design |
AN678 |
|
Click Here |
| MICROCHIP |
Transmitter |
Designing LF Talkback for a Magnetic Base Station |
AN912 |
|
Click Here |
| MICROCHIP |
Transmitter |
Magnetic Tuning of Resonant Sensors and Methods for Increasing |
AN832 |
|
Click Here |
| NORDIC SEMICONDUCTOR |
RF |
nRF9E5 RF and antenna layout |
nAN900-05 |
nRF9E5 |
Click Here |
| NORDIC SEMICONDUCTOR |
RF |
nRF905 RF and antenna layout |
nAN900-04 |
nRF905 |
Click Here |
| NXP SEMICONDUCTORS |
RF |
CLTV663 Antenna design guide |
AN11019 |
|
Click Here |
| NXP SEMICONDUCTORS |
Transmitter |
MIFARE Plus Card Coil Design |
AN10841 |
|
Click Here |
| NXP SEMICONDUCTORS |
Transmitter |
13.56 MHz RFID Proximity Antennas |
|
MF RC500 |
Click Here |
| NXP SEMICONDUCTORS |
Transmitter |
Micore Reader IC Family; Directly Matched Antenna Design |
|
MF RC500 |
Click Here |
| NXP SEMICONDUCTORS |
RF Amplifier |
RF Amplifier for NXP Contactless Reader IC's |
|
|
Click Here |
| NXP SEMICONDUCTORS |
Transmitter |
MIFARE ISO/IEC 14443 PICC Selection |
|
|
Click Here |
| NXP SEMICONDUCTORS |
RF |
AN 1629 UHF RFID Label Antenna Design |
AN 1629 |
|
Click Here |
| NXP SEMICONDUCTORS |
RF |
AN Micore Reader IC Family; Directly Matched Antenna Design |
|
|
Click Here |
| NXP SEMICONDUCTORS |
RF |
AN1491 Directly matched Antenna - Excel calculation |
AN1491 |
|
Click Here |
| STMICROELECTRONICS |
Memory |
Communication protocols on the LRI64 long range RFID memory IC |
AN2234 |
LRI64 |
Click Here |
| STMICROELECTRONICS |
RF |
How to design a 13.56 MHz customized tag antenna |
AN2866 |
CRX14 |
Click Here |
| STMICROELECTRONICS |
RF |
Antenna (and associated components) matching-circuit calculation for the CRX14 coupler |
AN1806 |
|
Click Here |
| STMICROELECTRONICS |
Memory |
RFID library for SR176 tag management with STR71x |
AN2399 |
CRX14 |
Click Here |
| TEXAS INSTRUMENTS |
RFID Transmitter |
Antenna Matching for the TRF7960 RFID Reader |
|
TRF7960 |
Click Here |
| TEXAS INSTRUMENTS |
RFID Transmitter |
Using the SPI Interface with TRF7960 |
|
TRF7960 |
Click Here |
| TEXAS INSTRUMENTS |
RFID Transmitter |
Implementation of ISO14443B Protocol in the TI TRF796x |
|
TRF796x |
Click Here |
| TEXAS INSTRUMENTS |
RFID Transmitter |
Implementation of ISO15693 Protocol in the TI TRF796x |
|
TRF796x |
Click Here |
| TEXAS INSTRUMENTS |
RFID Transmitter |
Implementation of ISO14443A Anti-Collision Sequence in the TI TRF796x |
|
TRF796x |
Click Here |
| TEXAS INSTRUMENTS |
RFID Transmitter |
Firmware Description of the TI TRF796x Evaluation Module (EVM) |
|
TRF796x |
Click Here |
| TEXAS INSTRUMENTS |
RFID Transmitter |
SRD Antennas |
AN003 |
|
Click Here |
| TEXAS INSTRUMENTS |
RFID Transmitter |
Compact 868/915 MHz Antenna Design |
|
|
Click Here |
| TEXAS INSTRUMENTS |
RFID Transmitter |
CC11xx Sensitivity versus Frequency Offset and Crystal Accuracy |
|
CC11xx |
Click Here |
| NORDIC SEMICONDUCTOR |
RF |
Benefits of Total Integration of Large RF Circuits |
Click Here |
| NORDIC SEMICONDUCTOR |
RF |
Debugging nRF24EX/nRF9E5 programs using the Keil uVision2 debugger |
Click Here |
| NORDIC SEMICONDUCTOR |
RF |
Design-in of RF circuits |
Click Here |
| NORDIC SEMICONDUCTOR |
RF |
Tuning the nRF24xx matching network |
Click Here |
| FREESCALE SEMICONDUCTOR |
MCU |
MC9S08LL16 MCU offers 70 percent reduction |
Click Here |
| Manufacturer |
Product Type
| White Paper Title
| URL |
| ATMEL |
RF |
RFID Transponder demo |
TMEB8704 |
|
Click Here |
| ATMEL |
RF |
Atmel LF-RFID Kit Comparison Chart |
ATAK2270 |
|
Click Here |
| ATMEL |
RF |
KIT, RFID APPLICATION, 125KHZ |
ATA2270-EK1 |
|
Click Here |
| ATMEL |
RF |
ATmega128RFA1 Evaluation Kit |
ATAVR128RFA1-EK1 |
|
Click Here |
| AVONWOOD |
RFID |
Eureka 125kHz RFID Starter Kit - RS232 Reader Module |
EUR111K4907 |
|
Click Here |
| AVONWOOD |
RFID |
Eureka 125kHz RFID Starter Kit - USB Desktop Reader |
EUR111K4909 |
|
Click Here |
| AVONWOOD |
RFID |
Eureka 13.56MHz RFID Starter Kit - RS232 Reader Module |
EUR211K4910 |
|
Click Here |
| AVONWOOD |
RFID |
Eureka 13.56MHz RFID Starter Kit - USB Desktop Reader |
EUR211K4912 |
|
Click Here |
| AVONWOOD |
RFID |
Eureka UHF Passive RFID Starter Kit-USB Desktop Reader |
EURUHFK4913 |
|
Click Here |
| AVONWOOD |
RFID |
Eureka UHF Passive RFID Starter Kit-USB Desktop Reader |
EURUHFK4915 |
|
Click Here |
| AVONWOOD |
RFID |
RFID Wakeup Unit System |
EURIDK4933 |
|
Click Here |
| FREESCALE SEMICONDUCTOR |
MCU |
S08LL Demonstration Board |
DEMO9S08LL16 |
MC9S08LL16 |
Click Here |
| FREESCALE SEMICONDUCTOR |
MCU |
TWR-S08LL64 Tower System 8-bit Segment LCD Module |
TWR-S08LL64-KIT |
MC9S08LL64 |
Click Here |
| FREESCALE SEMICONDUCTOR |
MCU |
QE8 Demonstration board |
DEMO9S08QE8 |
MC9S08QE8CLC |
Click Here |
| FREESCALE SEMICONDUCTOR |
MCU |
DEMO9S08JM16 Lab tutorials |
DEMO9S08JM16 |
MC9S08JM16 |
Click Here |
| MICROCHIP |
RF |
2.4 GHz 802.11b Low Power Transceiver Module |
ZG2100M/ZG2101M |
|
Click Here |
| MICROCHIP |
MCU |
MPLAB Starter Kit for PIC18F MCU |
DM180021 |
PIC18F |
Click Here |
| MICROCHIP |
MCU |
PIC18 Explorer Board |
DV164136 |
PIC18F |
Click Here |
| MICROCHIP |
MCU |
Explorer 16 Development Board |
DM240001 |
PIC24F |
Click Here |
| MICROCHIP |
MCU |
Explorer 16 Starter Kit |
DV164033 |
PIC24F |
Click Here |
| MICROCHIP |
MCU |
PICDEM™ 4 Demonstration Board |
DM163014 |
PIC18F1320 |
Click Here |
| NXP SEMICONDUCTORS |
RFID |
KIT EVAL MIFARE RFID 13.56MHZ |
MFEV700/HAB,122 |
|
Click Here |
| OLIMEX |
RFID |
RFID Reader, 125KHZ, USB Interface |
MOD-RFID125 |
|
Click Here |
| OLIMEX |
RFID |
MOD, USB RFID Reader for 125KHZ Tags |
MOD-RFID125-BOX |
|
Click Here |
| OLIMEX |
RFID |
RFID Tags for MOD-RFID125 |
RFID125-KEY |
|
Click Here |
| OLIMEX |
RFID |
RFID Tags for MOD-RFID125 |
RFID125-CSH |
|
Click Here |
| OLIMEX |
RFID |
RFID board EB052-00-1 |
EB052 |
|
Click Here |
| RF SOLUTIONS |
RFID |
RF Receiver Decoder |
RDF1-433 |
|
Click Here |
| RF SOLUTIONS |
RFID |
Mifare RFID Receiver Module + Integrated Antenna & serial output |
RWD-MIFARE-OEM |
|
Click Here |
| RF SOLUTIONS |
RF |
RFID reader evaluation board |
RSK100 |
|
Click Here |
| TEXAS INSTRUMENTS |
RFID |
TRF7960EVM Evaluation Module |
TRF7960 EVM |
|
Click Here |
| TEXAS INSTRUMENTS |
RFID |
Passive Low Frequency (PaLFI) Evaluation Kit |
EZ430-TMS37157 |
|
Click Here |
| TEXAS INSTRUMENTS |
RFID |
Stellaris® 13.56 MHz RFID Wireless Kit |
DK-EM2-7960R |
TRF7960 |
Click Here |
| TEXAS INSTRUMENTS |
RFID |
The RI-RFM-007B radio frequency power module |
RI-RFM-007B |
|
Click Here |
| TEXAS INSTRUMENTS |
RFID |
134.2 kHz intelligent module |
RI-STU-MRD1-30 |
|
Click Here |
| TEXAS INSTRUMENTS |
RFID |
Low Frequency Micro Evaluation Kit |
RI-K3A-001A-00 |
|
Click Here |
| TEXAS INSTRUMENTS |
RF |
Stellaris® 2.4 GHz SimpliciTI Wireless Kit |
DK-EM2-2500S |
|
Click Here |
| TEXAS INSTRUMENTS |
RF |
Stellaris® 13.56 MHz RFID Wireless Kit |
DK-EM2-2520Z |
|
Click Here |
| TEXAS INSTRUMENTS |
RFID |
Antenna tuning indicator,RFID, S2000 |
RI-ACC-ATI2-00 |
|
Click Here |
| TEXAS INSTRUMENTS |
MCU |
MSP430FG4618/F2013 Experimenter Board |
MSP-EXP430FG4618 |
MSP430FG4618 |
Click Here |
| TEXAS INSTRUMENTS |
MCU |
MSP430 MCU Optimization for Ultra-Low Power: Clocks, Low Power modes, and Intelligent Peripherals |
MSP430 |
Click Here |
| ATMEL |
RF Transmitter |
2.4G Radio Transceiver for IEEE802.15.4 and ZigBee Applications |
|
Click Here |
| ATMEL |
RF Transmitter |
Low Frequency RFID Reader IC |
U2270B |
Click Here |
| MICROCHIP |
RF Transceiver |
ISM Band Sub-GHz RF Transceiver |
|
Click Here |
| TEXAS INSTRUMENTS |
RF Transceiver |
RFID Solution Based on TRF7960 & MSP430Fx |
TRF7960 |
Click Here |
| FREESCALE SEMICONDUCTOR |
RF Transceiver |
Solution on Remote Keyless Entry for Automotive Application |
|
Click Here |
This is tab 6