Nowadays radio communication technologies have been widely spread in many areas such as commercial, military, and meteorological. The traditional radio communication systems are built with hardware dedicated to specific applications that require different frequencies, bandwidths, modulation modes and coding protocols. As communication technology keeps evolving, the hardware-based implementation method is presenting noticeable disadvantages in terms of cost, production cycle, and compatibility. In order to avoid these disadvantages, a new conception called software-defined radio (SDR) technology has been introduced. [+MORE]
SDR technology enables a general-purpose hardware platform to realize compatibility with different wireless communication systems by updating software configurations. It brings flexibility to radio systems, allowing adding new functions and upgrading system easily.
SDR systems could be implemented based on either RF sampling or IF sampling. The former sampling method directly converts RF signal into digital one so that the analog circuitry section could be reduced as much as possible. However this method results in high implementation difficulty because RF sampling needs extreme-high-speed A/D converters and DSPs. The latter sampling method is the popular one at present. It firstly converts RF signal down to IF signal, which is then sampled for digitalization. Although the method is compromised in terms of flexibility, the requirements on devices’ performance are greatly reduced and the implementation becomes much easier.
The hardware of a SDR system basically consists of antenna, RF front-end, ADCs, DACs, and a DSP. In order to cover a wider frequency band, a wide-band antenna or multiple antennas could be used. The RF front-end conducts a series of work including filtering, up and down conversion, power amplification, and low-noise amplification. The ADC operates in the receiving chain of the system to perform analog-to-digital conversion, while the DAC is located in the transmission chain for digital-to-analog conversion. Both ADC and DAC must feature sufficient operation bandwidth and speed to satisfy Nyquist sampling rate. In order to relieve the work load of the DSP, a DDC (Digital Down Converter) device can be used to convert the output of ADC into base-band so as to reduce data transfer speed. The similar device, DUC (Digital Up Converter), could also be used in the transmission chain for the same purpose. Another option for this functionality is using a FPGA as the substitute for DDC and DUC. The DSP is responsible for base-band signal processing such as modulation/demodulation, anti-interference and FEC (Forward Error Correction).
Moreover, modern communication systems usually adopt non-constant envelope modulation which commonly requires power amplifiers running in their linear regions, resulting in lower efficiency. Running the amplifiers in their non-linear regions could obtain higher efficiency, but a dedicated chip or a FPGA should be added before power amplifier to implement CFR (Crest Factor Reduction) and DPD (Digital Pre-Distortion) on signals.[-LESS]
Hover over the blocks to view more recommended solutions.
| |
 |
AD8339-EVALZ
ANALOG DEVICES
The AD8339 board illustrates the capabilities of the demodulator with programmable phase shifter. AD8339 is a key component of a phase shifter system that aligns time-skewed information contained in RF sigmnals. The AD8339 can be configured using the software provided with the board, or using an external digital pattern generator via the 20-pin flat-cable connector. |
|
| |
 |
CFTL-CN0134-EVALZ
ANALOG DEVICES
This circuit is an implementation of the analogue portion of a broadband transmitter - analogue baseband in / RF out. Its designed to evaluate CN0134, utilizing ADF4350, a fully integrated fractional-N PLL IC, that behaves as a local oscillator, upconverting analogue I/Q signals to RF. |
|
| |
 |
EVAL-AD5504EBZ
ANALOG DEVICES
This is an evaluation board for AD5504 allowing the user to fully evaluate all the functions and performance of the device prior to designing it into a system. The evaluation board can be used in a standalone mode with control coming from an external DSP or microcontroller, or it can be connected to a PC using the USB cable supplied with the evaluation board kit. Software is provided that allows the user to program the various registers of the AD5504 with ease. |
|
| |
 |
AD9284-250EBZ
ANALOG DEVICES
This is a fully featured board that supports various modes of operation for the AD9284 Analogue-to-Digital Converter with application software.
|
|
| |
 |
KSZ8873MLL-EVAL
MICREL SEMICONDUCTOR
The Kit allows for development with KSZ8873MLL, an integrated 3-port switch on a chip , designed to enable 10/100Mbps switch systems, with advanced power management with energy detect mode that shuts the transceiver down when a port is idle.
|
|
| |
| ALTERA |
FPGA |
Tool Flow for Design of Digital IF for Wireless Systems |
AN442 |
Cyclone III |
Click Here |
| ALTERA |
FPGA |
Digital IF Modem Design with the DSP Builder Advanced Blockset |
AN544 |
|
Click Here |
| ALTERA |
FPGA |
Accelerating DUC & DDC System Designs for WiMAX |
AN421 |
|
Click Here |
| ALTERA |
FPGA |
Crest Factor Reduction |
AN396 |
|
Click Here |
| ALTERA |
FPGA |
Crest Factor Reduction for OFDMA Systems |
AN475 |
|
Click Here |
| ANALOG DEVICES |
DAC/ADC |
Multicarrier CDMA2000 Feasibility |
AN808 |
AD9779A |
Click Here |
| ANALOG DEVICES |
DAC/ADC |
Multicarrier TD-SCDMA Feasibility |
AN0974 |
AD9779A |
Click Here |
| ANALOG DEVICES |
DAC |
Understanding High Speed DAC Testing and Evaluation |
AN928 |
|
Click Here |
| ANALOG DEVICES |
ADC |
Understanding High Speed ADC Testing and Evaluation |
AN835 |
|
Click Here |
| ANALOG DEVICES |
ADC |
Little Known Characteristics of Phase Noise |
AN741 |
|
Click Here |
| ANALOG DEVICES |
ADC |
A WiMax Double Downconversion IF Sampling Receiver Design |
AN851 |
AD9246 |
Click Here |
| ANALOG DEVICES |
DDC |
A WiMax Double Downconversion IF Sampling Receiver Design |
AN851 |
AD6636 |
Click Here |
| ANALOG DEVICES |
DUC |
The Advantages of Using a Quadrature Digital Upconverter (QDUC) in Point-to-Point Microwave Transmit Systems |
AN-0996 |
AD9857 |
Click Here |
| ANALOG DEVICES |
DDC |
Basics of Designing a Digital Radio Receiver |
|
|
Click Here |
| AVAGO TECHNOLOGIES |
LNA |
LNA Design with the MGA-16516 Matched Pair, Low Noise Amplifier |
AN5441 |
MGA-16516 |
Click Here |
| AVAGO TECHNOLOGIES |
LNA |
LNA Design with the MGA-17516 Matched Pair, Low Noise Amplifier |
AN5442 |
MGA-17516 |
Click Here |
| AVAGO TECHNOLOGIES |
LNA |
MGA-633P8 GaAs MMIC LNA Enables 900 MHz BTS Amplifier with Industry Best Noise Figure and Linearity |
AN5457 |
MGA-633P8 |
Click Here |
| AVAGO TECHNOLOGIES |
LNA |
MGA-635P8 GaAs ePHEMT MMIC 2.5 GHz Low Noise Amplifier with Superior Noise and Linearity Performance |
AN5479 |
MGA-635P8 |
Click Here |
| AVAGO TECHNOLOGIES |
LNA |
Using the MGA-87563 GaAs MMIC in Low Noise Amplifier Applications in the 800 Through 2500 MHz Frequency Range |
AN1116 |
MGA-87563 |
Click Here |
| AVAGO TECHNOLOGIES |
RF Amplifier |
High Linearity Wireless Data Power Amplifier for 2.3 to 2.5 GHz Applications |
AN5468 |
MGA-43228 |
Click Here |
| AVAGO TECHNOLOGIES |
RF Amplifier |
High Linearity Wireless Data Power Amplifier for 2.5 to 2.7 GHz Applications |
AN5469 |
MGA-43328 |
Click Here |
| AVAGO TECHNOLOGIES |
RF Amplifier |
AVT-50663 / 52663 Darlington Amplifier for Broadband Application (DC to 6GHz) |
AN5473 |
AVT-50663/52663 |
Click Here |
| AVAGO TECHNOLOGIES |
RF Amplifier |
AVT-51663 / 53663 Darlington Amplifier for Broadband Application (DC to 6GHz) |
AN5474 |
AVT-51663/53663 |
Click Here |
| AVAGO TECHNOLOGIES |
Mixer |
Using the AMMP-6530 in Upconverter Applications from 6 GHz through 28 GHz |
AN5276 |
AMMP-6530 |
Click Here |
| AVAGO TECHNOLOGIES |
Mixer |
AMMP-XXXX, Production Assembly Process |
AN5386 |
AMMP-XXXX |
Click Here |
| AVAGO TECHNOLOGIES |
Mixer |
The IAM-93516 for 1.9 GHz Down converter for Cellular Infrastructure Application with Integrated IF Amplifier |
AN5112 |
IAM-93516 |
Click Here |
| FREESCALESEMICONDUCTOR |
RF Amplifier |
General Purpose Amplifier and MMIC Biasing |
AN3100 |
|
Click Here |
| FREESCALESEMICONDUCTOR |
RF Amplifier |
Thermal Measurement Methodology of RF Power Amplifiers |
AN1955 |
|
Click Here |
| INTERSIL |
DDC |
Use of HSP50216 QPDC for CDMA Applications (IS-95 and CDMA2000) |
AN9928 |
HSP50216 |
Click Here |
| INTERSIL |
DDC |
Use of HSP50216 and ISL5216 QPDC in Wideband Applications - UMTS |
AN9927 |
HSP50216 |
Click Here |
| LATTICE SEMICONDUCTOR |
FPGA |
Multi-Channel Digital Up/Down Converter for WiMAX Systems |
RD1052 |
LatticeECP2M-35 |
Click Here |
| LATTICE SEMICONDUCTOR |
FPGA |
Digital Radio Transmission |
ATL-DIGTRX-01 |
Click Here |
| LINEAR TECHNOLOGY |
Mixer |
Signal Chain Noise Analysis for RF-to-Digital Receivers |
DN439 |
|
Click Here |
| LINEAR TECHNOLOGY |
Mixer |
Fast Time Division Duplex (TDD) Transmission Using an Upconverting Mixer with a High Side Switch |
DN480 |
|
Click Here |
| TEXAS INSTRUMENTS |
DSP |
Small Form Factor Software-Defined Radio Development Tools |
SPRT406A |
|
Click Here |
| TEXAS INSTRUMENTS |
DAC/ADC |
Smart Selection of ADC/DAC Enables Better Design of Software-Defined Radio |
SLAA407 |
|
Click Here |
| ALTERA |
FPGA |
DSP-FPGA System Partitioning for MIMO-OFDMA Wireless Basestations |
Click Here |
| ALTERA |
FPGA |
Implementing Digital IF & Digital Predistortion Linearizer Functions with Programmable Logic |
Click Here |
| ALTERA |
FPGA |
Crest Factor Reduction for OFDM-Based Wireless Systems |
Click Here |
| ALTERA |
FPGA |
Designing With Confidence for Military SDR Production Applications |
Click Here |
| ALTERA |
FPGA |
Architecture and Component Selection for SDR Applications |
Click Here |
| LATTICE SEMICONDUCTOR |
FPGA |
LatticeECP/EC FPGAs: A Systolic Array Processor for Software Defined Radio |
Click Here |
| LATTICE SEMICONDUCTOR |
FPGA |
FPGAs in Next Generation Wireless Networks |
Click Here |
| LATTICE SEMICONDUCTOR |
FPGA |
The FPGA As A Flexible And Low-Cost Digital Solution For Wireless Base Stations |
Click Here |
| TEXAS INSTRUMENTS |
DAC |
Principles of Data Acquisition and Conversion |
Click Here |
| Manufacturer |
Product Type
| White Paper Title
| URL |
| ANALOG DEVICES |
DAC |
Using the AD9708/AD9760/AD9762/AD9764-EB Evaluation Board |
AD9764-EB |
AD9764 |
Click Here |
| ANALOG DEVICES |
DUC |
1 GSPS Quadrature Digital Upconverter with 14-Bit DAC Evaluation Board |
|
AD9957 |
Click Here |
| INTERSIL |
DAC |
HI5x60EVAL1 User’s Manual |
HI5x60EVAL1 |
HI5960 |
Click Here |
| INTERSIL |
DAC |
HI5760EVAL1 Evaluation Board User’s Manual |
HI5760EVAL1 |
HI5760 |
Click Here |
| TEXAS INSTRUMENTS |
DSP |
SFF SDR Evaluation Module |
|
|
Click Here |
| TEXAS INSTRUMENTS |
DAC |
DAC5675A Evaluation Module User Guide |
|
DAC5675A |
Click Here |
| TEXAS INSTRUMENTS |
DAC |
TSW4200 Demonstration Kit User's Guide |
TSW4200 |
DAC3283 |
Click Here |
| TEXAS INSTRUMENTS |
DAC |
DAC3283 EVM User's Guide |
DAC328x EVM |
DAC3283 |
Click Here |
| TEXAS INSTRUMENTS |
DAC |
DAC5668/88/89 EVM User's Guide |
DAC5688 EVM |
DAC5688 |
Click Here |
| TEXAS INSTRUMENTS |
DAC |
TSW4100EVM User's Guide |
TSW4100 |
DAC5688 |
Click Here |
| TEXAS INSTRUMENTS |
ADC |
ADS61x9/55xxEVM User's Guide |
ADS5545 EVM |
ADS5545 |
Click Here |
| TEXAS INSTRUMENTS |
ADC |
ADS64XX EVM User's Guide |
ADS6425 EVM |
ADS6425 |
Click Here |
| ALTERA |
FPGA |
Accelerating OFDMA-MIMO Wireless System Design |
|
Click Here |
| ALTERA |
FPGA |
Cyclone III FPGA Overview Part1 |
Cyclone III |
Click Here |
| ALTERA |
FPGA |
Cyclone III FPGA Overview Part2 |
Cyclone III |
Click Here |
| ALTERA |
FPGA |
Stratix FPGA Overview |
Stratix |
Click Here |
| LINEAR TECHNOLOGY |
Mixer |
Study on 0.4GHz to 2.7GHz High Linearity Upconverting Mixer |
LT5578 |
Click Here |
| NATIONAL SEMICONDUCTOR |
ADC |
ADC16V130 16-bit, 130 MSPS Reference Subsystem Overview |
ADC16V130 |
Click Here |
| NATIONAL SEMICONDUCTOR |
ADC |
National's Communications Infrastructure Solutions Optimize System Efficiency |
|
Click Here |
| TEXAS INSTRUMENTS |
ADC |
Improving the Power Efficiency of High-Speed ADCs |
|
Click Here |
| TEXAS INSTRUMENTS |
ADC |
ADS6425 Podcast |
ADS6425 |
Click Here |
This is tab 5
This is tab 6